This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: PBTL / BTL mode output configuration

Part Number: TPA3255


Hello,

In PBTL mode, outputs A and C / B and D are connected with each other. Would it also be possible to connect  A and D / B and C and configure the chip in BTL with the two input pairs externally connected with the same signal, but one invers in phase, e.g. Input A and D Input + / Input B and input C -?

Or, in other words, does the choice of configuration "PBTL" or "BTL" changed more than just the input routing? Because otherwise you could always get a PBTL by BTL and corresponding wiring of the inputs. Or am I wrong?

Best,

Ralf