This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3221: Audio forum

Part Number: TPA3221


 I am using the TPA3221 on a 2 sided PCB with a layout similar to the Evaluation board and following all the recommendations in the application note. It is set up in the 30dB gain mode as a master in a stereo BTL . .configuration in  AD mode. Power supply voltage is 27 volts.  VDD, AVDD, and GVDD are supplied by an external 5V supply. 

Using a 100 Hz sine as input, the output shows a slight non-linearity fixed at the +/- 1 volt level . It is audible, around 1% distortion.  It is independent of load. The power supply voltage has an effect, but the magnitude does not change significantly from 12 to 28 volts. 

This non-linearity repeats around +/- 6 volts but is a smaller proportion of the waveform at that level.

Any thoughts would be appreciated.