Hi,
I have a very annoying problem with Purepath v1.88 build 3 (which I think is the latest for TAS3308?)
In one of my designs I am using several splitters (12) based on the component Split_TI_v2 and one of them generates an error in the design file so when it opens all blocks until this splitter is opened and then the following error is displayed (and the rest after this is ignored):
(build language Danish) "Objektreferencen er ikke indstillet til en forekomst af et object"
which means "the Object reference is not set for an instance of an object"
if I manually removes the object from the .pfw file the file opens (of course with the splitter missing) but no errors except for warnings for unconnected inputs and outputs where the splitter should have been. If I save and load again - no problems, and the design also builds without problems if I add in the splitter again (no matter what number I give it). As soon as I save with the splitter in the design the problem reverts and I can't load the design again...
Is this a know error, a limitation in size, number of splitters and is there an updated version of Purepath I am not aware of?
Best regards
Jes Mosgaard