This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5242RHBEVM: [PCM5242RHBEVM] PPC2 ERROR message "swap bit failure on hardware -- Please check device "

Part Number: PCM5242RHBEVM

What should I do?

Configuration :

thanks

  • Hi,

    I am not sure about that error.  Though it might have something to do with your configuration.  Are you trying to supply an external I2S input to the device? If that is the case you have your jumper wires and jumper shunt in the wrong position.  The jumpers should be totally removed, and the external source should be connected to the center post of the I2S bypass headers (JP1-4).

    It is possible that you are shorting the I2S outputs of the EVM by connecting them to an external source.

    Thanks,

    Paul

  • I made a mistake........

    thanks reply