Hello, our customer is facing following issue at new product design.
(1) As the datasheet said,
BKND_ERR REGISTER (0x1C)
When a back-end error signal is received from the internal power stage, the power stage is reset, stopping all
PWM activity. Subsequently, the modulator waits approximately for the time listed in Table 18 before attempting
to re-start the power stage.
In this function what type of error is detected at the internal power stage? Is that single function of 4.5A over current detection or another back-end error situation would be detected?
They have seen this error at low temperature environment only. Can we get TAS5719 OCP threshold temperature characteristics?
(2) VOLUME CONFIGURATION REGISTER (0x0E)
D7 D6 D5 D4:1 0 0 1 – – – Reserved
However they had been using :1111 on previously produced equipment. From now nobody know the reason why they had changed TI Reserved setting.
What is the function of 0X0E D6 and D5 register setting? Is that test mode or something?
Regards,
Mochizuki