This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3107: 1. Global Headset function 2. Amp power>2W function support needed device

Part Number: TLV320AIC3107


Hi team,

Is there any codec support as below ? Because TLV320AIC3107 can not meet the requirement.

1. Global Headset function

2. Amp power>2W

  • Hello Oliver,

    1. Are you referring to AHJ and OMTP detection? If so, unfortunately, our codecs do not automatically detect which connection is being used. TI offers an autonomous headset switch (TS3A226AE) that can be used in this case. 

    2. The AIC3120 and AIC3100 offer amp power > W. I should note that these are Mono ADC and Stereo DAC Codecs.

    Regards,

    Aaron