I need some assistance in reducing the TLV320AIC3104 when the line outputs are turned on. It sounds like white noise. Here's the configuration, I have a master and slave unit which operate using the CC8520 Pure Path Wireless SOIC. The master has a differential mic input on the MIC1R channel of a AIC3104 and the slave's AIC3104 is configured such that the received signal is outputted onto both the left and right line outs differentially. When the slave first powers up, the outputs are nice and quite, but when the master pairs, the outputs turn on and the noise is heard. Even after turning off my master, the noise is still heard, even though I power down the line outputs going from active to low-power on the CC8520 (although this may not be occurring since it seems the outputs are still active with no signal.)
Unused inputs to the AIC3104 are floating. Do I need to capacitively couple them to ground even though the inputs are not powered?
The mic gain on the master is set to 20dB. Only a highpass filter is used with a cut off at 1Hz.
The output gain on the slave is set to 0dB gain on both left and right DACs, and 9dB gain on both the left and right line outs. I don't have a filter set at this time in the slave.
Any recommendations?
Thanx,
Denis