This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6166A2: Question of Detection Range of OMTP/CTIA Jacks and I2C Code Review of the TPA6166 Amplifier

Part Number: TPA6166A2
Other Parts Discussed in Thread: TS3A227E,

Hi Sirs,

We are designing the TPA6166 with an OEM customer. Here we have two questions which need product line's support:

1. WOuld you please advise if the TPA6166 detect OMTP and CTIA jacks based on the same impedance range of the TS3A227E device?

TPA6166 datasheet:


  

TS3A227E specification:



2. Can we bring up the TPA6166 to support OMTP/CTIA jack detection function with the following I2C instructions?

-----------------------------------------------------------------
w 80 1E 19 #Enable Registers 3
w 80 04 EE #Interrupt Mask Register 1
w 80 05 F4 #Interrupt Mask Register 2
w 80 07 B9 #Left Headphone Volume Register
w 80 08 79 #Right Headphone Volume Register
w 80 09 47 #Microphone/Ground Control
w 80 12 01 #Reserved Registers
w 80 13 45 #Reserved Registers
w 80 1A 95 #Jack Detect AC Test Settings
w 80 1E 01 #semi auto mode
w 80 1D 80 #Enable Registers 2
-----------------------------------------------------------------

Thank you and Best regards,

Wayne Chen
07/16/2020