This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TAS2563: What Tuning Tools are Available for TAS2563 in PPC3

Part Number: TAS2563


For TAS2563, under "Tuning and Audio Processing" of PPC3, what are those tuning tools used for?

Specifically:

  1. Smart Amp Protection
  2. Equalizer
  3. Dynamic Range Compression
  4. Dynamic Equalizer

  • The tuning and processing tools available for TAS2563 are Smart Amp Protection, 5-band equalizers, 2-band dynamic range compression, and dynamic equalizer.

    In Smart Amp Protection:

    • Users can adjust the corner frequency and the filter type of the high pass filter and tune the protection algorithm of each band in terms of priority and speed of thermal and excursion protection
    • Example of using a different excursion priority values may improve bass performance

    In 5-bands Equalizers:

    • There are total of 5 biquad filters for users to tune according to their preference of speaker output frequency response.
    • Example of Treble Shelf Filter to boost treble performance

    In 2-bands Dynamic Range Compression:

    • Users can map the input/output response to to avoid output clipping or high frequency artifacts due to high amplitude input signals of a specific frequency range
    • Example of using DRC a extreme ratio as hard limiter to compress the dynamic range of the loud signals
    • Example of Noise Gate in DRC page to attenuate audio signal that is below -60 dBFS

    In Dynamic Equalizer:

    • Users can compress loud signal at a specific frequency without affecting the frequency response of quieter audio signal.
    • Example of DEQ to de-compensate resonant frequency peak

    For more information about device tuning, please refer to the Smart Amp Tuning Guide, and the TAS2563 Tuning Guide