Part Number: TAS5342LA
Hello,
I get a very loud noisy output at the PWM outputs of the TAS5342LA when part starts getting a little bit too warm. The weird thing is, both protection signals OTW and SD stay high, but when I cool down the part with coolant spray this behavior stops. Also the IC temperature I'm measuring is around 60°C wich is way below max specs.
I designed the BTL stage as provided in SLAU243 (M1,M2,M3 = 0) All Caps close to the Chip are X7R. Roc =22kOhm.
The picture below shows the two PWM inputs (Channel 1 and 2) and the TAS5342LA PWM output (Channel3) directly at the Output pin before the Filter inductor. I'm measuring with a 4Ohm load.
Any Ideas what could cause this problem?
Thanks in advance!