This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul,
Hi,
Somehow embedded image is not visible in your post.
Can you please attach it again? Also our apps engineer responsible for this device is on vacation. Please expect a delay in response.
Regards,
AK
Hi,
Applications engineer responsible for this device is on vacation. Please expect a delay in response.
Regards,
AK
Hi Gust,
You can use multiple volume control components in a single flow. This would set the "baseline" value. For example, you could set the line-out volume to be -3dB, and the analog output to be -6dB. Now if you write -6dB to page0, R61 and R62 registers, the line out volume would be -9dB and the analog output volume would be -12dB.
Thanks,
Paul