Other Parts Discussed in Thread: PCM1808, PCM1860, PCM1803, PCM1802, PCM1804, PCM1860-Q1
Hello,
My customer was wondering how they should do for the existing system working at Fs=16kHz with system clock of 768fs in slave mode. They'd like to use PCM1808-Q1 as it is without changing their SW, but it doesn't seem to support 768fs. How would you say for this use case? Do you have an IC supporting this use case? Note that they prefer HW control.
One of the solution would be using external 1/2 divider for the system clock to make it 384fs from 12.288MHz to 6.144MHz if it doesn't support 768fs. Do you think it works with PCM1808-Q1? If it does, what do they have to check? The datasheet just shows the Figure 22, but does it all they have to check for the timings? I mean aren't there any timing requirements between SCKI and I2S pins?
3603.SlaveModeTimingRequirements.docx
Best Regards,
Yoshikazu Kawasaki