Other Parts Discussed in Thread: SRC4392,
Hi Expert,
Can the SRC4392 on the PP-SALB2-EVM configured as master mode on the board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
Can the SRC4392 on the PP-SALB2-EVM configured as master mode on the board?
Hello,
The SRC team is not familiar enough with the overall operation of the PP-SALB2-EVM to confirm if it will be possible or not with the available software, but the fundamental connections (see post below) should allow for this operation as the I2C and ASI connections, including MCLK are accessible.
HI Collin,
Thanks for replying me. What about I2S? Could customer use I2S master mode with SRC4392?