Hi team,
I would like to share control command through I2C for the project using PCM6340 and the other project using PCM6360.
I plan to send a command to set the register which only exists in PCM6360 (ex Addr:0x0F ASI_CH5) to PCM6340 too.
1. How does PCM6340 device react when I send a command to 0x0F ASI_CH5? Will it return NACK?
2. Addr:0x73 D[2:3] is setting for CH5/6. Should I make it "Disable" if I use PCM6340 or is it OK to leave it default?
3. If I need to set "disable" to above 0x73 D[2:3] register, Is there a possibility that the device return NACK?
regards,