Hi team,
Dynamic channel pupd enable feature prohibit power down Channel 1 as below.
"1d = Channel can be powered up or down individually, even if channel
recording is on. Do not powered-down channel 1 if this bit is set to '1'"
But from the DYN_MAXCH_SEL[1:0] register description below, Channel 1 and Channel 2 seems to be power down dynamically.
Is my understanding wrong?
"Dynamic mode maximum channel select configuration.
0d = Channel 1 and channel 2 are used with dynamic channel power-up,
power-down feature enabled"
regards,