Other Parts Discussed in Thread: PCM1808
Hello,
My questions are related to the post shown below which asked for antialiasing filter.
1) The antialiasing filter cut off frequency is shown on page 4 as -3dB at 1.3MHz when it is Fs=48kHz, but is it the same for other frequencies? For example, will it be like 430kHz at Fs=16kHz?
2) Is it possible to provide the frequency response curve? My customer would like to know if it is -12dB/oct, -18dB/oct or others.
3) Would you please tell me the reason why it is set to -3dB at 1.3MHz? My customer would like to design external peripheral circuit for noise reduction by the information.
/t/559956?tisearch=e2e-sitesearch&keymatch=PCM1808
Best Regards,
Yoshikazu Kawasaki