This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA2505: Asking for PGA2505 SPI control

Part Number: PGA2505

Hi Team,

Customer uses PGA2505 on the new project. Would you please review and provide comment for the questions?

1. customer used PGA2505 and PGA2505 was controlled this chip via SPI bus;

2. PGA2505 will affect the system SPI bus in our system as follows:

a. R290 mounted, System SPI_CLK's high level is about 1V(abnormal);

b. After remove R290, System SPI_CLK's high level recovered to 3V3;

 

Have you met this issue before? or Would you give us some comments about it?

BR,

SHH