This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4674A: Power Consumption

Part Number: LM4674A

Dear Sir,

We are estimating the playback time for a battery operating product.

When VDD = 3.6V, the total power consumption (excluding power use for sound producing) is typically 4mA for 8 ohm speakers.

If two speakers are drawing 2mA each to produce sound, the total power consumption of the LM4674A is typically 4+2+2 = 8mA. Am I correct? Is there other power consumption I need to consider?