Hi Team,
From the TAS6424M-Q1 datasheet, the absolute maximum rating of VDD is only 3.5V, is there any tolerance? In my point of view, if maximum recommended condition is 3.5V, the absolute maximum rating should be higher, right?
Because our front-end buck may generate 3.8V voltage spike on VOUT when voltage cranking, I am worried that the VDD of TAS6424M-Q1 may be damaged.
Could we guarantee the VDD can endure 3.8V spike in 50us?
Regards,
Roy