Hi team,
In Slave mode, what happens if BCK and LRCLK rise time and fall time do not meet 20ns?
It is assumed that the other interface timings can be satisfied with a margin.
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
In Slave mode, what happens if BCK and LRCLK rise time and fall time do not meet 20ns?
It is assumed that the other interface timings can be satisfied with a margin.
regards,
Hi,
Excessive rise and fall times can lead to an increase in the jitter since the edge may be sampled at slightly different points in time and this will degrade the noise performance of the device. It may also lead to somewhat higher power consumption on the digital rail. This device will be more sensitive to jitter since it does not include an integrated PLL, so if possible I would recommend using a clock buffer that can satisfy these timing requirements.
Best,
Zak