This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5508C: automute control register 0x14

Part Number: TAS5508C

Hello

My customer is using TAS5508C and in the market.

It may be special case, but  customer has pop issue from the market

in case very low level sound with low volume .

So far, customer had been set 0x14 as 14h [ D4=1].

When customer tested 0x14h as 04h [D4=0], pop with automute improved.

Do you agree?”

In TAS5508C data sheet , ”Set input automute threshold less than bit 1 (zero input signal), lowest automute threshold."

in booth of the D4=1, D=0 case.

Best Regards