Part Number: PP-SALB-EVM
I can't seem to get the hardware checks to pass.
Looking at other people that have the same problem, I appear to have everything set up ok.
Any ideas as to what I am doing wrong?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PP-SALB-EVM
I can't seem to get the hardware checks to pass.
Looking at other people that have the same problem, I appear to have everything set up ok.
Any ideas as to what I am doing wrong?
The problem is with a PP-SALB-EVM. I also have a PurePath Console Motherboard + TAS5766MRMTEVM which is working fine.
Since yesterday, I installed the software on another Win 10 machine and it works fine there with the PP-SALB-EVM so it isn't a hardware issue. Using both machines I'm basically up and running but it would be nice to sort the problem on my main machine so I can connect to both dev boards.
Thanks Colin
Hi Colin,
PP-SALB_EVM requires Line Properties - Advanced - Default format to 44100Hz, otherwise, PurePath Console Motherboard + TAS5766MRMTEVM needs set the value to 48000Hz.
So you need to manually change this property when switching different EVM board.
Rdgs,
Matthew