Part Number: SRC4382EVM-PDK
Other Parts Discussed in Thread: SRC4382, SRC4392
Hi
I am struggling to install the USB drivers for the SRC4382EVM-PDK.
I have followed the instructions in the User guide (section 3.3), but the device is recognized as a Human interface device, not a NI-VISA USB device as the guide says is required.
the USB-MODEVM_WDM.inf file is in the C:/Windows/inf directory, and is installed, but when I try to update the driver, USB-MODEVM does not appear as an option.
Where am i going wrong?
I have tried on both windows xp and windows 10 32bit, the result is the same on both.
Thanks
Ben