Other Parts Discussed in Thread: TLV320ADC3140, , TLV320ADC6140
Hello,
What are the requirements for the MCLK clock signal input to the TLV320ADC5140, TLV320ADC3140, and TLV320ADC6140 when operating as an Audio master with an external MCLK input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What are the requirements for the MCLK clock signal input to the TLV320ADC5140, TLV320ADC3140, and TLV320ADC6140 when operating as an Audio master with an external MCLK input?
1.) The maximum input frequency is: 36.864MHz.
2.) Duty-Cycle min/max is 45% and 55% respectively
3.) Jitter should be <1ns if the PLL will be used with the MCLK as an input
4.) Logic level glitches or other noise on the clock input must be avoided. Glitches may trigger a clock error which will shut down the ASI. Please keep the MCLK input signal as clean as possible by adding some series resistance (10-33 Ohms) near the output drivers, avoiding long adjacent trace routing with other switching signals, and possibly adding some shunt capacitance if the glitches are sourced extrinsically.