I have a PCM5100 and I need to change the word (LRCK) and bit (BICK) clock sample frequency to match the master componet. I've tested the PCM5100 and it work correctly when using a PC as audio input and I was able to hear the audio from the speaker connected to the DAC. However when I try to connect the master component (BT module) of my circuit using PCM interface I get digital signal to the DAC input but no analog output. I've compared the sample frequency of LRCK and BICK of the DAC when working with PC and with BT module and the frequencies are different. According to the datasheet of the PCM5100 it should support the frequencies below:
LRCK 16KHz
BICK 256KHz
I need to know how to change the sample frequency of the PCM and make this work with my circuit.