This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: Input Reference Power

Part Number: LMX2595
Other Parts Discussed in Thread: LMX2592

What is the recommend input power for the input reference signal (Oscin) for double and single-ended input signal? Assume the 50 ohm input configuration shown in Figure 32 of the datasheet.

  • Hi Scott,

    We recommend no more than 2Vpp at the pin (10dBm single-ended, 13dBm differential). However, it depends on what kind of OSCin signal you have. The 10dBm single-ended / 13dBm differential number is for sine-wave input. Sine wave input slew rate scales as a function of input amplitude, so actually the best case for sine wave input is the maximum input power, always. For our own validation we use a 16dBm Wenzel sine-wave OCXO into a 3dB attenuator and a balun. On the other hand, if you have a high slew rate signal like LVDS, LVPECL, or CML at the reference input, the input power becomes less important. Between a 200mVpp signal and a 2Vpp signal with the same slew rate, there is not much difference in noise performance unless there is some concern about noise immunity or amplitude margin.

    Regards,

    Derek Payne

  • Hi Derek, Sorry I had the wrong part number. My part is LMX2592 and Table 6.1 of the datasheet shows  <1.8 Vpp with Vcc applied and <1Vpp with Vcc = 0. My input is 100 MHz sine wave. So, based on your explanation above, I should have an input close to 1.8Vpp assuming Vcc is applied. Thanks, Scott

  • Scott,

    I think so, because my Table 6.1 does not constrain input reference.

    Datasheet pulled directly from https://www.ti.com/lit/ds/symlink/lmx2595.pdf

    My recommendation comes from section 6.5:

    Regards,

    Derek Payne