Part Number: CDCVF2310
Hi Jennifer,
Thanks again for your answers.
I would like to ask:
1. How do I calculate the minimum serial resistor that will keep current bellow rating of +/- 50mA,
Is it 3.3V/ 50mA? 3.3V/ 100mA ? else ?
I guess the "dark side" of this approach is having a termination resistor out of SI rules (>>50ohm) , no?
2. How comes a larger resistor is better for SI? The RC will increase and rise time will increase.
Are you "afraid" the OSC increased output current will ruin the clock SI? It can drive 12mA, 3.3V/ 2.5K =~ 1.5mA should not be a problem, no ?
looking forward to hear from you
Thanks
Amnon