Part Number: LMX2594
Hi,
We are developing precision Location measurement unit. In that we are using two LMX2594 to generate four output clocks of 452.95MHz, used as ADC clock inputs. The first LMX IC's two clock outputs are given to one set of ADCs, and another LMX IC outputs are given to another set of ADCs in RFSoC.
We need to know the clock output stabilization time of the LMX2594, so that we will start sampling the ADCs after this time period to avoid seeing phase misaligned values. Also we can be little confident that both chip outputs are stable. I cannot find it from the datasheet. Could you please provide this detail.?
Thanks,
Pradeep. S