Hello
Please tell me how to output CLKout without control during Power-On.
Please support.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Please tell me how to output CLKout without control during Power-On.
Please support.
Hi Shimawaki,
As per the datasheet section 8.6.2, default POR register values, all CLKout are powerdown.
But POR default sets OSCout to buffered OSCin and format to LVPECL, which can be used as clock during power-on.
Please also see: https://e2e.ti.com/support/clock-and-timing/f/48/p/839075/3103205
Regards,
Ajeet Pal
Hi Ajeet Pal,
Thank you for your support.
Is there a way to output CLKout0-13 without setting from SPI after Power-On?
Is it possible to program to turn on CLKout0-13 after Power-On using TICS Pro etc.?
Regards,
SHIMAWAKI
Hi Shimawaki,
CLKout0-13 are not possible to turn-on without programming after POR.
TICS Pro is a tool, which program the device through SPI interface. Yes, after Power-on, you can program the device and make it enable CLKout0-13 using TICS Pro.
Regards,
Ajeet Pal