Other Parts Discussed in Thread: MSP430F5529, USB2ANY
Hello
Currently, I manufactured LMX2594EVM (SV601308) and the reference board (SV601349A) by referring to the circuit diagram and gerber that provided. As I know, reference board can be connected to the PC through a USB connection and controlled by a program called 'TICS PRO'. However, even with USB connection, 'TICS PRO' does not recognize the board.(In the program, it is displayed as 'Connection Mode: Device Not Connected'.)
I think 'TICS PRO' cannot recognize the MSP430F5529 Chip in the reference board, is there anything additional to do to use 'TICS PRO'?
Additionally, when the reference board was connected to the PC by usb connection, the voltage of the specific pins of the MSP430F5529 Chip was as follows.
pin no. 57: 0.1V , pin no. 58: 0.1V , pin no. 59: 0V , pin no. 60: 0V