Other Parts Discussed in Thread: LMK00804B
Hi,
We have TCXO CLK generator whose output is HCMOS and the output swing having VOL max of 0.1xVDD and VIHmin of 0.9xVDD. The VDD is 3.3V for both TCXO and LMK00804B.
We intend to drive the LVCMOS output of TCXO to LVCMOS_CLK input pin of LMK00804B.
Is there a concern as we do see that the recommended LVCMOS input level of LMK00804B has VIHmin of 2V and VILMax of 1.3V and the swing of TCXO is within the range?
Earlier the same approach was followed while using CDCLVC11XX IC instead of LMK00804B and it worked fine.
Pls clarify.
Thanks,
Ravi