Other Parts Discussed in Thread: LMK04832, LMK04821, LMK04133, LMK04033, , LMX2615-SP
For my design, I am trying to have the LMK04832 produce clock signals of speeds 1 GHz and 2 GHz. Now, the internal VCO0 produces frequencies in the range between 2440 and 2600 MHz, and VCO1 produces frequencies in the range between 2945 and 3225 MHz. These then are divided by whole integers into the 14 clock outputs. My question is because the clock dividers only divide by whole numbers, can I reach a frequency of 2 GHz? By my math, frequencies between 2.44 GHz and 1.6275 GHz (= 3.225 / 2) are unreachable. Or am I missing something in the datasheet.