Part Number: LMX2615-SP
Other Parts Discussed in Thread: MSP430FR5969, TPS7A4501-SP
Hello,
1. If I don't wanted to used PIN Mode and I have to controlled two LMX2615-SP with one controller MSP430FR5969 with following requirement then is it possible.?
a). We need phase synchronization between two output of two different LMX2615-SP.
2. What is the optimum input power level if we used fosc frequency 50 MHz.?
3. Below is the LMX2615 board output when DC is in off condition. (Note: This board developed by us)
4. Below is the LMX2615 board output when DC is in ON condition. (Note: This board developed by us)
during the ON Condition we got some low frequency hump.
Condition: Rest of the output port is 50 Ohm terminated.
Out of the two input we used only one and another one is terminated with 50 ohm.
Applied Voltage: 3.3 Volt and Current is 270 mA during ON condition.
What is the reason for low freq. hump and how to rectify the problem. ?