Part Number: CDCE949
Hello, we are using the CDCE949 with the following configuration. External crystal with 20MHz attached to the device, so crystal oscillator is used. VDD is 1.8V (+/-5%) and VDDOUT is 3.3V (+/-5%). The outputs are programmed as follows:
Y1: 40MHz, Y2: 33MHz, Y3: 25MHz, Y4-5 not used, Y6: 20MHz, Y7: 20MHz, Y8, Y9: 12.286MHz (each output). This means the usage of PLL1, 3 and 4 (PLL2 is unused). The critical clock is the 25MHz clock at Y3 with 25MHz.
What maximum jitter (p-p) can we expect at the output Y3 (25MHz)? According datasheet the jitter is specified 180 ps max if 4 PLLs are switching at Vddout=3.3V. If only one PLL is switching (Y2, Y3 outputs used) then the jitter is 100 ps maximum. Why is the jitter dependent from number of PLLs used? Is this caused by device internal crosstalk?
Thanks in advance!
Best regards Andreas N.