This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00304: Unused differential clock input left open

Part Number: LMK00304

We use the differential clock input CLKin0/CLKin0* and the pins of CLKin1/CLKin1* are left open.
Do you see any problem in doing so? Do we have a higher current consumption when that differential input CLKin1/CLKin1* is left open?
Datasheet states that CLKin input is biased at about 1.4V.

Many thanks
Udo