Part Number: LMK05028
Hi,
I also would like to ask you a question about DPLL Phase Lock Detectors as below.
Following my understanding is correct?
"The Lock ppm and Unlock ppm set here are deviations from the REF TDC Rate [Hz]."
For example, because the input deviation of IN0 is specified as ± 100ppm,
I set "DPLL Phase Lock Detectors"
Lock ppm: 100ppm
Unlock ppm: 200ppm
Is there any problem?
My understanding is
LOFL released at ± 100ppm or less
LOFL occurs at ± 200ppm or more
Is this correct?
And Also, I have set the default value to "Lock Ave" and "Unlock Ave".
That is to say,
Lock Ave: 10
Unlock Ave: 2
However, When DPLL LBW [Hz] is set to 10Hz, Are each Ave value (Lock Ave: 10/ Unlock Ave: 2) valid?
As the datasheet describes following,
"Higher averaging may be useful when locking to an input with high wander or when the DPLL is configured with a narrow loop bandwidth."
Let me ask you this question.
Thanks for your support.
Best Regards,
Takumi