Hi expert,
My ctm want to do AC coupling input for LMK00304 . I see below post saying there is internal biasing providing the input offset -0.3V. And I just want to confirm this internal biasing provides the common mode voltage for the input (VCMD>0.25V) so external biasing is not needed? And work well both for LVDS and HCSL signals? Thanks.