Part Number: LMX2820
Other Parts Discussed in Thread: LMK04832
Hi Team,
We are using LMK04832 and LMX2820 is our boards and we are facing PLL locking issue in LMX2820. The below image shows the clock architecture.
PFA the schematics of LMK04832 and LMX2820 of our design. And also find the attached LMK04832 and LMX2820 .tcs file
LMK04832 AND LMX2820 DESIGN.pdf
ADC_LMX2820_FPD_270MHz_2700output.tcs
DAC_LMX2820_FPD_270MHz_5400output.tcs
MS_LRDE_WBRFU_LMK04832_RF_Clock_clkin1.tcs
As per this design, We are not facing any issue and the LMK and LMX PLLs are locking properly.
We wanted to change the frequencies and hence we made required hardware changes and after that the LMX2820 PLL is not locking. PFA the .zip file for schematic of LMK04832 and LMX2820 for new frequency with loop filter and VCXO updated and also find the .tcs files and pllatinum sim file (Loop filters calculation).
LMK04832 and LMX2820 new frequency.zip
We have 6 boards and the hardware changes for new frequency is done on one board in that, CPOUT pin of LMX2820 measures 0 Volts. where as in other boards it measures 1.3 to 1.4 Volts (old frequency design)
what can be the cause for LMX2820 PLL not locking for the new frequency changes?
--
Regards
Kiran