Part Number: LMK04610
Hello,
I am having trouble getting the zero delay mode to work on the design I am trying to generate. In feedback mode (setting on PLL2 tab of TICS pro software) the PLL2 locks, and the output clocks are what I expect them to be. However if I switch it to OUTPUT5 or OUTPUT6 for zero delay mode, the output frequencies jump up ~4MHz and the PLL is no longer locked. I notice when I change this setting that the frequency in the PFD + LD box changes. Do I need to make the output of channel 5 or channel 6 match the output of the prescaler? What else do I need to consider for zero delay mode to operate?
Thanks,
Daniel