Part Number: LMK05318BEVM
Other Parts Discussed in Thread: LMK05318B
I also have a new LMK05318BEVM. Jumpers are set up as per the manual and the IIC is able to find the part but there is no output. The supply current is 220mA and all outputs are dead. There doesn't seem to be any DC CM bias on any of the differential outputs. But the Vdd output is correct. I tried changing the Vdd output from 3.3V to 1.8V but get the same thing. I have tried the default EVM program and versions that disabled all muting and syncing, but no outputs are active. Is this just a bad board? Thanks.