Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595
Hello. We are testing the LMX2595EVM with SMA100B. The frequency of reference clock from SMA100b is 100 MHz and Osc_doubler of LMX2595EVM is enabled. We find that at several frequencies, the measured phase noise at 1kHz and 10kHz offset do match what the data sheet specifices,but don‘t match the simulation results calculated by PLLatinum Sim. The comparison between measured results and simulation results are as follows.







It can be seen that at frequencies above, simulated results at 1kHz and 10kHz offset are much better than both measured results and specificed values of data sheet. Thus we think that the configuration we set in PLLatinum Sim might be unproper.
During operation of PLLatinum Sim, OSC noise is "data loaded" and the imported data is measured phase noise of 100 MHz reference clock from SMA100b. VCO noise and PLL noise are "Use Metrics", which are defult configuration. The loop filter is set according to the configuration in data sheet of LMX2595EVM.

Is there any possible reasons accounting for the mismatch between simulated results and measured results?