This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: LMX2820 4 single ended output configuration

Part Number: LMX2820


Hi,

Can we use 2 differential outputs (RFOUTA/B_P/N) of LMX2820 as 4 single ended RF outputs? In the datasheet, single ended output power is 3 dBm at 22 GHz when terminating compelement side of outputs with 50 ohm. Instead of terminating with 50 ohm, I want to use all 4 output pins as different channels. Is it possible to obtain 4 channel 3-dBm 22 GHz RF output with LMX2820?

Ali Bugra KORUCU