Part Number: LMK04808BEVAL
Other Parts Discussed in Thread: LMK04808, USB2ANY, LMK03806BEVAL, LMK04803, LMK04832, LMK04828
Hello there,
We are looking to buy LMK04808B eval board to make use of the PLL2 to generate 750MHz and 1GHz LVPECL outputs. I aiming to use it in a single-loop mode (PLL2, Internal VCO mode).
I've used TICS-Pro to generate a configuration for the same using 500MHz OSCin (based on our application) - see the config file attached. My questions/concerns are following, please if you could help:
1. As I understood - PLL2's VCO output feeds back to PLL1 in Dual-loop mode. Does this still applicable in single-loop mode?LMK04808_500MHz_In_750MHz_1GHz_out_single_loop.tcs
The configuration I did - gives the warning about PLL1's VCO freq and PLL2's reference don't match

Do I need to worry about this warning - as I want to use it in single-loop mode (PLL2 only) and don't necessarly need PLL1-lock
2. Do we need to buy USB2ANY device seperately, or Is it included in the eval kit?