Part Number: LMX2582EVM
Hi,
I'm unable to change the frequency on LMX2582EVM. It always seems to be stuck on 3.62 GHz, irrespective of what you specify on the software. Here are the steps I followed.
1. Reset the registers
2. FcalEn = On
3. Set the frequency on the PLL section of the software
4. Load registers
So, I was wondering if there is any user guide for the TICS Pro software. If not, could someone help me with the steps to change the frequency?
I have two of these modules, and both have the same issue, so it can't be the hardware.
Thank you!