This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: SPI Readable Registers?

Part Number: LMX2594

I have written a python script that use spidev to write my TICS generated export TXT file to my LMX2549.  I write all of the registers and I seem to have my LMX2549 generating the correct clock outputs, however, I then want to readback those registers.  I read back a few registers and they are as expected, however, other registers do not match what I wrote via TICs.  From the datasheet, it appeared to me that ever register was read/write - able.  I was expecting to readback what I wrote to verify.  Are there write-only registers in the LMX2594?  Also, it seems that TICs knew what the fixed bits were for each registers so it wrote a 1 to where it was a fixed one or a 0 where it was 0 which was nice, however some registers are reading back as 0x00 and I clearly wrote a non-zero value.  This leads me to believe that perhaps some registers are write only or I wrote to them but then they are some status register and the value changed to 0.  I am trying to figure out a good routine to verify that I wrote my TICs content properly to the chip and I am looking for some help in this regard.

Thank you,

-Nathan