Part Number: LMX2594PSEVM
Other Parts Discussed in Thread: LMX2594
I would like to add one LMX2594PSEVM in Fig.2 to the LMX2594PSEVM Evaluation Kit in Fig.1 and perform the following evaluation while synchronizing four LMX2594s.
See attached file for illustration.
Inquiry about LMX2594PSEVM Evaluation Kit..pdf
①phase adjustment
I want to synchronize the four LMX2594s and adjust the phase or delay time of each of the four LMX2594s.
②Amplitude adjustment
I want to adjust the amplitude of each of the four LMX2594s while synchronizing the four LMX2594s.
③frequency adjustment
Keeping 4 LMX2594s in sync and adjusting the frequency of each 4 LMX2594
I want the LMX2594 to oscillate at different frequencies.
Is it possible to perform experiments ① to ③ using this LMX2594PSEVM Evaluation Kit and one LMX2594PSEVM?