Part Number: CDCLVC1108
Hi,
I am currently designing with a CDCLVC1108 to distribute clock signals to other devices. Not all outputs are going to be used, so I need to know exactly how they must be terminated so that they don't affect the circuit.
The device is powered with 3.3V. As per the datasheet, I would think that a resistor divider from Vdd to GND of 100 Ohms + 100 Ohms would fit.
Is this right? Please, provide the detailed info.
Also, for used outputs, do we need also this termination at receiver circuit side?
Best regards,
Salvador