Hi,
I have a multi-LMK04832 setup where each LMK is taking in the same 10MHz clock as its reference clock (matched cables, etc) and has a 100MHz external VCXO.
The device in dual PLL with nested 0-delay mode, FB_MUX = SYSREF.
It is creating the following clocks:
- 10MHz clocks (SYSREF)
- 100 MHz clocks
I have the following questions:
1.)If I need 100MHz in-phase between different outputs of the same LMK, does SYNC be required?
2.)If the 100MHz output between different LMKs needs to be in the same phase, does SYNC be required?
Thanks!