Part Number: LMX2820
Other Parts Discussed in Thread: LMX2594, LMX2594EVM,
Hello team.
I'm working with the LMX2820.
When I'm working in standard mode everything works just fine.
I'm trying to improve its phase noise, so I operated the LOOPBACK_EN.
The wanted frequency is 10GHz.
At first, I'm locking the LMx2820 to 10GHz in standard mode with no issue. RFOUTB is applied to Mini-Circuits mixer.
I'm using the LMX2594 at 7.6GHz as an LO and apply it to the Mini-Circuits mixer and apply its IF 2.4GHz output to the RFin of the LMX2820 while enabling the LOOPBACK_EN.
I'm changing R10 to 0X1000 ; R36 to 0x37 and R34 to 0x810.
The problem I'm having is that the LMX2820 loose lock and jumps to 10.1GHz.
Please help.