Other Parts Discussed in Thread: CDCDB800, CDCDB400
If not using SMBUS, can the CKPWRGD_PD# pin be left no connect (and pulled low via 180K pulldown)?
Or should it be pulled high?
The pin configuration section states "If unused, the pin can be left no connect."
However, "Table 8-2. OE[7:0]# Functionality" seems to imply that if CKPWRGD_PD# is low, the output will not run.
Please advise.
Thanks,